AIN#.OFFSET
Description
AIN#.OFFSET sets the analog offset, which is added to the analog input command to the drive. This value compensates for the analog input signal (AIN#.VALUE) offset or drift.
-
- AIN#.ZERO will set this value.
Examples
Code
--> AIN1.VALUE 0.056 V --> AIN1.OFFSET -0.056 --> AIN1.VALUE 0.000 V
Context
For more information see Analog Input.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
| Type | Read/Write |
| Units | V |
| Range | -10V to +10V |
| Default Value | 0 V |
| Data Type | Float |
| See Also | |
| Stored in Non-Volatile Memory | Yes |
Variants Supported
All variants are supported.
Fieldbus Information
Fieldbus Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
AIN1.OFFSET |
3780h |
05h |
Signed16 |
- |
1000:1 |
Read/Write |
No |
|
AIN2.OFFSET |
3781h |
05h |
Signed16 |
- |
1000:1 |
Read/Write |
No |
|
Name |
ID |
Hex |
Data Type |
Access |
Units |
|---|---|---|---|---|---|
|
AIN1.OFFSET |
23050 |
5A0A |
Signed16 |
Read/Write |
- |
|
AIN2.OFFSET |
23051 |
5A0B |
Signed16 |
Read/Write |
- |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
AIN1.OFFSET |
23050 |
Float |
Read/Write |
- |
|
AIN2.OFFSET |
23051 |
Float |
Read/Write |
- |